Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static BendInsertDesignBuilder.BlankPositions |
BendInsertDesignBuilder.BlankPositions.PUNCH_PLATE
the blank is on the punch plate
|
static BendInsertDesignBuilder.BlankPositions |
BendInsertDesignBuilder.BlankPositions.STRIPPER_PLATE
the blank is on the stripper plate
|
Modifier and Type | Method and Description |
---|---|
BendInsertDesignBuilder.BlankPositions |
BendInsertDesignBuilder.blankPosition()
Returns the blank position in punch plate or stripper plate.
|
static BendInsertDesignBuilder.BlankPositions |
BendInsertDesignBuilder.BlankPositions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BendInsertDesignBuilder.BlankPositions |
BendInsertDesignBuilder.BlankPositions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BendInsertDesignBuilder.BlankPositions[] |
BendInsertDesignBuilder.BlankPositions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BendInsertDesignBuilder.setBlankPosition(BendInsertDesignBuilder.BlankPositions blankPosition)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.