Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DieBaseBuilder.SplitMethod |
DieBaseBuilder.SplitMethod.SINGLE_PLATE
select single plate
|
static DieBaseBuilder.SplitMethod |
DieBaseBuilder.SplitMethod.WHOLE_SUB_DIEBASE
select whole sub-diebase
|
Modifier and Type | Method and Description |
---|---|
DieBaseBuilder.SplitMethod |
DieBaseBuilder.splitSubSingle()
Returns the split options: whole sub die base or single plate.
|
static DieBaseBuilder.SplitMethod |
DieBaseBuilder.SplitMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieBaseBuilder.SplitMethod |
DieBaseBuilder.SplitMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieBaseBuilder.SplitMethod[] |
DieBaseBuilder.SplitMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieBaseBuilder.setSplitSubSingle(DieBaseBuilder.SplitMethod splitSubSingle)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") OR nx_engineering_die_wizard ("NX Engineering Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.