Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Method and Description |
---|---|
SelectReuseLibraryListItemBuilder |
SelectReuseLibraryListBuilder.createListItem()
Generate a list item.
|
SelectReuseLibraryListItemBuilder |
SelectReuseLibraryListItemBuilderList.findItem(int index)
Returns the object at the input index.
|
SelectReuseLibraryListItemBuilder[] |
SelectReuseLibraryListItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SelectReuseLibraryListItemBuilderList.append(SelectReuseLibraryListItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
SelectReuseLibraryListItemBuilderList.append(SelectReuseLibraryListItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SelectReuseLibraryListItemBuilderList.erase(SelectReuseLibraryListItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
SelectReuseLibraryListItemBuilderList.erase(SelectReuseLibraryListItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SelectReuseLibraryListItemBuilderList.findIndex(SelectReuseLibraryListItemBuilder obj)
Finds the index where the input object appears.
|
void |
SelectReuseLibraryListItemBuilderList.insert(int location,
SelectReuseLibraryListItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
SelectReuseLibraryListItemBuilderList.setContents(SelectReuseLibraryListItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
SelectReuseLibraryListItemBuilderList.swap(SelectReuseLibraryListItemBuilder object1,
SelectReuseLibraryListItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.