Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static EjectorPostProcessingBuilder.TrimPartName |
EjectorPostProcessingBuilder.TrimPartName.NOTRIMPART
No trim part
|
Modifier and Type | Method and Description |
---|---|
EjectorPostProcessingBuilder.TrimPartName |
EjectorPostProcessingBuilder.trimPart()
Returns the trim part in which trim surface features are cycled.
|
static EjectorPostProcessingBuilder.TrimPartName |
EjectorPostProcessingBuilder.TrimPartName.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EjectorPostProcessingBuilder.TrimPartName |
EjectorPostProcessingBuilder.TrimPartName.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EjectorPostProcessingBuilder.TrimPartName[] |
EjectorPostProcessingBuilder.TrimPartName.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EjectorPostProcessingBuilder.setTrimPart(EjectorPostProcessingBuilder.TrimPartName trimPart)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.