Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static RunSimulationBuilder.CollisionCheckOptions |
RunSimulationBuilder.CollisionCheckOptions.FACET_BODY_DISTANCE
Measure facet bodies distance to do collision check
|
static RunSimulationBuilder.CollisionCheckOptions |
RunSimulationBuilder.CollisionCheckOptions.MESH_TRIANGLE_INTERSECTION
Mesh facet body, check the mesh triangle intersection or not
|
static RunSimulationBuilder.CollisionCheckOptions |
RunSimulationBuilder.CollisionCheckOptions.SOLID_BODY_INTERSECTION
Get the solid body, use intersection boolean result to do collision check
|
Modifier and Type | Method and Description |
---|---|
RunSimulationBuilder.CollisionCheckOptions |
RunSimulationBuilder.collisionCheckOption()
Returns the collision check method option
License requirements: None. |
static RunSimulationBuilder.CollisionCheckOptions |
RunSimulationBuilder.CollisionCheckOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RunSimulationBuilder.CollisionCheckOptions |
RunSimulationBuilder.CollisionCheckOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RunSimulationBuilder.CollisionCheckOptions[] |
RunSimulationBuilder.CollisionCheckOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RunSimulationBuilder.setCollisionCheckOption(RunSimulationBuilder.CollisionCheckOptions collisionCheckMethod)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.