Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DieCavityAndSlugHoleBuilder.BottomPlateSlugItems |
DieCavityAndSlugHoleBuilder.BottomPlateSlugItems.CIRCLE
Bottom plate slug type is circle
|
static DieCavityAndSlugHoleBuilder.BottomPlateSlugItems |
DieCavityAndSlugHoleBuilder.BottomPlateSlugItems.CLEARANCE
Bottom plate slug type is clearance
|
static DieCavityAndSlugHoleBuilder.BottomPlateSlugItems |
DieCavityAndSlugHoleBuilder.BottomPlateSlugItems.FILLET
Bottom plate slug type is fillet
|
static DieCavityAndSlugHoleBuilder.BottomPlateSlugItems |
DieCavityAndSlugHoleBuilder.BottomPlateSlugItems.MICKEY
Bottom plate slug type is mickey
|
static DieCavityAndSlugHoleBuilder.BottomPlateSlugItems |
DieCavityAndSlugHoleBuilder.BottomPlateSlugItems.NONE
Bottom plate slug type is none
|
static DieCavityAndSlugHoleBuilder.BottomPlateSlugItems |
DieCavityAndSlugHoleBuilder.BottomPlateSlugItems.RECTANGLE
Bottom plate slug type is rectangle
|
static DieCavityAndSlugHoleBuilder.BottomPlateSlugItems |
DieCavityAndSlugHoleBuilder.BottomPlateSlugItems.SLOT_HOR
Bottom plate slug type is slot horizontal
|
static DieCavityAndSlugHoleBuilder.BottomPlateSlugItems |
DieCavityAndSlugHoleBuilder.BottomPlateSlugItems.SLOT_VER
Bottom plate slug type is slot vertical
|
Modifier and Type | Method and Description |
---|---|
DieCavityAndSlugHoleBuilder.BottomPlateSlugItems |
DieCavityAndSlugHoleBuilder.normalBottomBackPlateSlug()
Returns the normal bbpslug
License requirements: None. |
static DieCavityAndSlugHoleBuilder.BottomPlateSlugItems |
DieCavityAndSlugHoleBuilder.BottomPlateSlugItems.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieCavityAndSlugHoleBuilder.BottomPlateSlugItems |
DieCavityAndSlugHoleBuilder.BottomPlateSlugItems.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieCavityAndSlugHoleBuilder.BottomPlateSlugItems[] |
DieCavityAndSlugHoleBuilder.BottomPlateSlugItems.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieCavityAndSlugHoleBuilder.setNormalBottomBackPlateSlug(DieCavityAndSlugHoleBuilder.BottomPlateSlugItems normalBottomBackPlateSlug)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.