Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static ScrapDesignBuilder.EditScrapType |
ScrapDesignBuilder.EditScrapType.APPLY_MINIMUM_RADIUS
Applies minimum radius to sharp corners of scraps
|
static ScrapDesignBuilder.EditScrapType |
ScrapDesignBuilder.EditScrapType.CHANGE_STATION
Changes the station number of scraps
|
static ScrapDesignBuilder.EditScrapType |
ScrapDesignBuilder.EditScrapType.DELETE
Deletes scraps
|
static ScrapDesignBuilder.EditScrapType |
ScrapDesignBuilder.EditScrapType.MERGE
Merges two scraps into one
|
static ScrapDesignBuilder.EditScrapType |
ScrapDesignBuilder.EditScrapType.SPLIT
Splits a scrap by selected curves
|
static ScrapDesignBuilder.EditScrapType |
ScrapDesignBuilder.EditScrapType.UPDATE
Updates scraps if there is any design change
|
Modifier and Type | Method and Description |
---|---|
ScrapDesignBuilder.EditScrapType |
ScrapDesignBuilder.editMethod()
Returns the edit method, which includes splitting, merging, applying minimum radius, changing station, deleting and updating
License requirements: None. |
static ScrapDesignBuilder.EditScrapType |
ScrapDesignBuilder.EditScrapType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ScrapDesignBuilder.EditScrapType |
ScrapDesignBuilder.EditScrapType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ScrapDesignBuilder.EditScrapType[] |
ScrapDesignBuilder.EditScrapType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ScrapDesignBuilder.setEditMethod(ScrapDesignBuilder.EditScrapType editMethod)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.