public interface DieDesignSettingBuilder extends Builder
DieDesignSettingBuilder
This class is for Die Design Setting UI
DieDesignSettingCollection.createDieDesignSettingBuilder()
Property | Value |
---|---|
RoundoffInsertXYPosition | 1 |
Modifier and Type | Method and Description |
---|---|
boolean |
roundoffInsertXYPosition()
Returns the option to roundoff insert X and Y position
License requirements: None. |
void |
setParameters(String[] paraNames,
String[] paraValues)
Set the parameter number, names and values in the tree list into builder attribute.
|
void |
setRoundoffInsertXYPosition(boolean roundoffInsertXYPosition)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
void setParameters(String[] paraNames, String[] paraValues) throws NXException, RemoteException
paraNames
- an array of namesparaValues
- an array of valuesNXException
RemoteException
boolean roundoffInsertXYPosition() throws NXException, RemoteException
NXException
RemoteException
void setRoundoffInsertXYPosition(boolean roundoffInsertXYPosition) throws NXException, RemoteException
roundoffInsertXYPosition
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.