Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static LsdynaGeometryPreparationBuilder.DrawType |
LsdynaGeometryPreparationBuilder.DrawType.DOUBLE_DRAW
For draw die, punch and binder are higher than die.
|
static LsdynaGeometryPreparationBuilder.DrawType |
LsdynaGeometryPreparationBuilder.DrawType.SINGLE_DRAW
For draw die, punch and binder are lower than die.
|
Modifier and Type | Method and Description |
---|---|
LsdynaGeometryPreparationBuilder.DrawType |
LsdynaGeometryPreparationBuilder.drawTypeOption()
Returns the draw type.
|
static LsdynaGeometryPreparationBuilder.DrawType |
LsdynaGeometryPreparationBuilder.DrawType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LsdynaGeometryPreparationBuilder.DrawType |
LsdynaGeometryPreparationBuilder.DrawType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LsdynaGeometryPreparationBuilder.DrawType[] |
LsdynaGeometryPreparationBuilder.DrawType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LsdynaGeometryPreparationBuilder.setDrawTypeOption(LsdynaGeometryPreparationBuilder.DrawType enumDrawType)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.