Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DieInsertBuilder.InsertModeItems |
DieInsertBuilder.InsertModeItems.BOUNDING_BOX
The die insert mode is bounding box
|
static DieInsertBuilder.InsertModeItems |
DieInsertBuilder.InsertModeItems.SKETCH_PROFILE
The die insert mode is sketch profile
|
static DieInsertBuilder.InsertModeItems |
DieInsertBuilder.InsertModeItems.STANDARD_INSERT
The die insert mode is standard insert
|
Modifier and Type | Method and Description |
---|---|
DieInsertBuilder.InsertModeItems |
DieInsertBuilder.insertMode()
Returns the insert mode
License requirements: None. |
static DieInsertBuilder.InsertModeItems |
DieInsertBuilder.InsertModeItems.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieInsertBuilder.InsertModeItems |
DieInsertBuilder.InsertModeItems.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieInsertBuilder.InsertModeItems[] |
DieInsertBuilder.InsertModeItems.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieInsertBuilder.setInsertMode(DieInsertBuilder.InsertModeItems insertMode)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.