public static class DieInsertBuilder.InsertModeItems extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BOUNDING_BOX
The die insert mode is bounding box
|
static int |
_SKETCH_PROFILE
The die insert mode is sketch profile
|
static int |
_STANDARD_INSERT
The die insert mode is standard insert
|
static DieInsertBuilder.InsertModeItems |
BOUNDING_BOX
The die insert mode is bounding box
|
static DieInsertBuilder.InsertModeItems |
SKETCH_PROFILE
The die insert mode is sketch profile
|
static DieInsertBuilder.InsertModeItems |
STANDARD_INSERT
The die insert mode is standard insert
|
Modifier and Type | Method and Description |
---|---|
static DieInsertBuilder.InsertModeItems |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieInsertBuilder.InsertModeItems |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieInsertBuilder.InsertModeItems[] |
values()
Returns an array that contains the values for this enum.
|
public static final DieInsertBuilder.InsertModeItems STANDARD_INSERT
public static final DieInsertBuilder.InsertModeItems SKETCH_PROFILE
public static final DieInsertBuilder.InsertModeItems BOUNDING_BOX
public static final int _STANDARD_INSERT
public static final int _SKETCH_PROFILE
public static final int _BOUNDING_BOX
public static DieInsertBuilder.InsertModeItems valueOf(int value)
public static DieInsertBuilder.InsertModeItems valueOf(String name)
public static DieInsertBuilder.InsertModeItems[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.