Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DieEngDefineProductOrientationBuilder.ViewDraftOptions |
DieEngDefineProductOrientationBuilder.ViewDraftOptions.COMPUTE_TRIM_ANGLES |
static DieEngDefineProductOrientationBuilder.ViewDraftOptions |
DieEngDefineProductOrientationBuilder.ViewDraftOptions.COMPUTE_WALL_ANGLES |
static DieEngDefineProductOrientationBuilder.ViewDraftOptions |
DieEngDefineProductOrientationBuilder.ViewDraftOptions.NONE |
Modifier and Type | Method and Description |
---|---|
static DieEngDefineProductOrientationBuilder.ViewDraftOptions |
DieEngDefineProductOrientationBuilder.ViewDraftOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieEngDefineProductOrientationBuilder.ViewDraftOptions |
DieEngDefineProductOrientationBuilder.ViewDraftOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieEngDefineProductOrientationBuilder.ViewDraftOptions[] |
DieEngDefineProductOrientationBuilder.ViewDraftOptions.values()
Returns an array that contains the values for this enum.
|
DieEngDefineProductOrientationBuilder.ViewDraftOptions |
DieEngDefineProductOrientationBuilder.visualizeDraftOptions()
Returns the visualize draft options
License requirements: die_engineering ("DIE ENGINEERING") . |
Modifier and Type | Method and Description |
---|---|
void |
DieEngDefineProductOrientationBuilder.setVisualizeDraftOptions(DieEngDefineProductOrientationBuilder.ViewDraftOptions visualizeDraftOptions)
License requirements: die_engineering ("DIE ENGINEERING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.