Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DieBaseBuilder.AlongDirectionOpt |
DieBaseBuilder.AlongDirectionOpt.ALONG_XDIRECTION
along X direction
|
static DieBaseBuilder.AlongDirectionOpt |
DieBaseBuilder.AlongDirectionOpt.ALONG_YDIRECTION
along Y direction
|
Modifier and Type | Method and Description |
---|---|
DieBaseBuilder.AlongDirectionOpt |
DieBaseBuilder.alongDirection()
Returns the direction options.
|
static DieBaseBuilder.AlongDirectionOpt |
DieBaseBuilder.AlongDirectionOpt.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieBaseBuilder.AlongDirectionOpt |
DieBaseBuilder.AlongDirectionOpt.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieBaseBuilder.AlongDirectionOpt[] |
DieBaseBuilder.AlongDirectionOpt.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieBaseBuilder.setAlongDirection(DieBaseBuilder.AlongDirectionOpt alongDirection)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") OR nx_engineering_die_wizard ("NX Engineering Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.