Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static StripLayoutBuilder.ToStationType |
StripLayoutBuilder.ToStationType.ONE
the end layout station is 1
|
static StripLayoutBuilder.ToStationType |
StripLayoutBuilder.ToStationType.THREE
the end layout station is 3
|
static StripLayoutBuilder.ToStationType |
StripLayoutBuilder.ToStationType.TWO
the end layout station is 2
|
Modifier and Type | Method and Description |
---|---|
StripLayoutBuilder.ToStationType |
StripLayoutBuilder.toStation()
Returns the To Station type on the Layout group of Strip Layout Design dialog
License requirements: None. |
static StripLayoutBuilder.ToStationType |
StripLayoutBuilder.ToStationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StripLayoutBuilder.ToStationType |
StripLayoutBuilder.ToStationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StripLayoutBuilder.ToStationType[] |
StripLayoutBuilder.ToStationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StripLayoutBuilder.setToStation(StripLayoutBuilder.ToStationType toStation)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.