Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static UserDefinedMotionBuilder.MotionTypes |
UserDefinedMotionBuilder.MotionTypes.LINEAR
Linear motion type
|
static UserDefinedMotionBuilder.MotionTypes |
UserDefinedMotionBuilder.MotionTypes.ROTARY
Rotary motion type
|
Modifier and Type | Method and Description |
---|---|
UserDefinedMotionBuilder.MotionTypes |
UserDefinedMotionBuilder.motionType()
Returns the motion type
License requirements: None. |
static UserDefinedMotionBuilder.MotionTypes |
UserDefinedMotionBuilder.MotionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static UserDefinedMotionBuilder.MotionTypes |
UserDefinedMotionBuilder.MotionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static UserDefinedMotionBuilder.MotionTypes[] |
UserDefinedMotionBuilder.MotionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
UserDefinedMotionBuilder.setMotionType(UserDefinedMotionBuilder.MotionTypes motionType)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.