Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static PunchInsertBuilder.NormalOffsetSideTypeItems |
PunchInsertBuilder.NormalOffsetSideTypeItems.DIE_SIDE
The offset side is die
|
static PunchInsertBuilder.NormalOffsetSideTypeItems |
PunchInsertBuilder.NormalOffsetSideTypeItems.PUNCH_SIDE
The offset side is punch
|
Modifier and Type | Method and Description |
---|---|
PunchInsertBuilder.NormalOffsetSideTypeItems |
PunchInsertBuilder.normalOffsetSide()
Returns the offset side option for normal pierce design.
|
static PunchInsertBuilder.NormalOffsetSideTypeItems |
PunchInsertBuilder.NormalOffsetSideTypeItems.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PunchInsertBuilder.NormalOffsetSideTypeItems |
PunchInsertBuilder.NormalOffsetSideTypeItems.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PunchInsertBuilder.NormalOffsetSideTypeItems[] |
PunchInsertBuilder.NormalOffsetSideTypeItems.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PunchInsertBuilder.setNormalOffsetSide(PunchInsertBuilder.NormalOffsetSideTypeItems normalOffsetSide)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.