Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static SpreadsheetDataParameter.Status |
SpreadsheetDataParameter.Status.FORCE_COLOR
If the parameter uses user value, normally it shows in UI in a different color.
|
static SpreadsheetDataParameter.Status |
SpreadsheetDataParameter.Status.HIDDEN_VALUE
The parameter has value, but it should be hidden to user
|
static SpreadsheetDataParameter.Status |
SpreadsheetDataParameter.Status.HIDE_STATUS
Not shown in UI
|
static SpreadsheetDataParameter.Status |
SpreadsheetDataParameter.Status.LOCK
User can't change the value in UI
|
static SpreadsheetDataParameter.Status |
SpreadsheetDataParameter.Status.MODIFIED
The parameter value is changed
|
static SpreadsheetDataParameter.Status |
SpreadsheetDataParameter.Status.NON_STANDARD_VALUE
The current value of this parameter is user's input, not from spreadsheet
|
static SpreadsheetDataParameter.Status |
SpreadsheetDataParameter.Status.OPTION_VALUE
The parameter has multiple value, but not treated as key parameter
|
static SpreadsheetDataParameter.Status |
SpreadsheetDataParameter.Status.READ_ONLY
This parameter is read only
|
static SpreadsheetDataParameter.Status |
SpreadsheetDataParameter.Status.SCALE_ITEM
This is a scale item
|
static SpreadsheetDataParameter.Status |
SpreadsheetDataParameter.Status.SHIP_RULE
This is used for ship design to trigger design.
|
static SpreadsheetDataParameter.Status |
SpreadsheetDataParameter.Status.SYSTEM_KEY
This is system key parameter
|
static SpreadsheetDataParameter.Status |
SpreadsheetDataParameter.Status.USER_KEY
Key parameter analyzed from spreadsheet search
|
Modifier and Type | Method and Description |
---|---|
static SpreadsheetDataParameter.Status |
SpreadsheetDataParameter.Status.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SpreadsheetDataParameter.Status |
SpreadsheetDataParameter.Status.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SpreadsheetDataParameter.Status[] |
SpreadsheetDataParameter.Status.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
boolean |
SpreadsheetDataParameter.hasStatus(SpreadsheetDataParameter.Status parameterStatus)
Check if the parameter has the given status
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.