Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static BurringInsertBuilder.ParentTypes |
BurringInsertBuilder.ParentTypes.CONTROL
use PDW project's control part as parent part
|
static BurringInsertBuilder.ParentTypes |
BurringInsertBuilder.ParentTypes.DIE
use PDW project's die part as parent part
|
static BurringInsertBuilder.ParentTypes |
BurringInsertBuilder.ParentTypes.DIE_BASE
use PDW project's die base part as parent part
|
static BurringInsertBuilder.ParentTypes |
BurringInsertBuilder.ParentTypes.SUB_DIE
use PDW project's sub-die base as parent part
|
Modifier and Type | Method and Description |
---|---|
BurringInsertBuilder.ParentTypes |
BurringInsertBuilder.parentPart()
Returns the parent part to create blank.
|
static BurringInsertBuilder.ParentTypes |
BurringInsertBuilder.ParentTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BurringInsertBuilder.ParentTypes |
BurringInsertBuilder.ParentTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BurringInsertBuilder.ParentTypes[] |
BurringInsertBuilder.ParentTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BurringInsertBuilder.setParentPart(BurringInsertBuilder.ParentTypes parentPart)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.