Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static MWMoldedPartValidationBuilder.CalculateOption |
MWMoldedPartValidationBuilder.CalculateOption.EDIT_REGIONS_ONLY
edit properties of region faces only
|
static MWMoldedPartValidationBuilder.CalculateOption |
MWMoldedPartValidationBuilder.CalculateOption.KEEP_EXISTING
calculate and keep existing properties on the faces
|
static MWMoldedPartValidationBuilder.CalculateOption |
MWMoldedPartValidationBuilder.CalculateOption.RESET_ALL
calculate and replace all properties for region faces
|
Modifier and Type | Method and Description |
---|---|
MWMoldedPartValidationBuilder.CalculateOption |
MWMoldedPartValidationBuilder.calculationOption()
Returns the calculation option on the Calculate Tab page.
|
static MWMoldedPartValidationBuilder.CalculateOption |
MWMoldedPartValidationBuilder.CalculateOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MWMoldedPartValidationBuilder.CalculateOption |
MWMoldedPartValidationBuilder.CalculateOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MWMoldedPartValidationBuilder.CalculateOption[] |
MWMoldedPartValidationBuilder.CalculateOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MWMoldedPartValidationBuilder.setCalculationOption(MWMoldedPartValidationBuilder.CalculateOption calculationOption)
License requirements: ug_mold_design ("UG MOLD") OR ug_prod_des_advisor ("Product Design Advisor") OR prog_die_wizard ("UG/Progressive Die Wizard") OR die_engineering ("DIE ENGINEERING") OR ug_die_design ("Die Design") OR nx_electrode_wizard ("NX Electrode Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.