Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static LsdynaGeometryPreparationBuilder.ContactType |
LsdynaGeometryPreparationBuilder.ContactType.AUTOMATIC_SURFACE_TO_SURFACE
The draw components contact type is automatic surface to surface.
|
static LsdynaGeometryPreparationBuilder.ContactType |
LsdynaGeometryPreparationBuilder.ContactType.FORMING_ONE_WAY_SURFACE_TO_SURFACE
The draw components contact type is forming one way surface to surface.
|
static LsdynaGeometryPreparationBuilder.ContactType |
LsdynaGeometryPreparationBuilder.ContactType.FORMING_ONE_WAY_SURFACE_TO_SURFACE_SMOOTH
The draw components contact type is forming one way surface to surface smooth.
|
static LsdynaGeometryPreparationBuilder.ContactType |
LsdynaGeometryPreparationBuilder.ContactType.FORMING_SURFACE_TO_SURFACE
The draw components contact type is forming surface to surface.
|
static LsdynaGeometryPreparationBuilder.ContactType |
LsdynaGeometryPreparationBuilder.ContactType.FORMING_SURFACE_TO_SURFACE_SMOOTH
The draw components contact type is forming surface to surface smooth.
|
static LsdynaGeometryPreparationBuilder.ContactType |
LsdynaGeometryPreparationBuilder.ContactType.SURFACE_TO_SURFACE
The draw components contact type is surface to surface.
|
Modifier and Type | Method and Description |
---|---|
LsdynaGeometryPreparationBuilder.ContactType |
LsdynaGeometryPreparationBuilder.contactTypeOption()
Returns the contact type.
|
static LsdynaGeometryPreparationBuilder.ContactType |
LsdynaGeometryPreparationBuilder.ContactType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LsdynaGeometryPreparationBuilder.ContactType |
LsdynaGeometryPreparationBuilder.ContactType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LsdynaGeometryPreparationBuilder.ContactType[] |
LsdynaGeometryPreparationBuilder.ContactType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LsdynaGeometryPreparationBuilder.setContactTypeOption(LsdynaGeometryPreparationBuilder.ContactType enumContactType)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.