public interface BaseFEModel extends IFEModel
FENode
) and Elements (FEElement
) in the model.
Only one instance of this class will exist in each assyfem part file
BaseFemPart.baseFEModel()
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
boolean |
askUpdatePending()
This method will inform caller if the finite element model is in an update pending state or not.
|
BeamSectionCollection |
beamSections()
Returns the Beam Section collection belonging to the part .
|
BoltCollection |
bolts()
Returns the connection collector manager belonging to the part .
|
CAEConnectionCollection |
caeConnections()
Returns the connection collector manager belonging to the part .
|
CaeReuseLibrary |
caeReuseLibrary()
Returns the CaeReuseLibrary belonging to the part .
|
CfdAutoRefinementConstraintCollection |
cfdAutoRefinementConstraints()
Returns the fluid domain automatic refinement constraint collection belonging to this fem part .
|
CfdContactPreventionConstraintCollection |
cfdContactPreventionConstraints()
Returns the fluid domain contact prevention constraint collection belonging to this fem part .
|
CfdLocalResolutionConstraintCollection |
cfdLocalResolutionConstraints()
Returns the fluid domain local resolution constraint collection belonging to this fem part .
|
ElementCollection |
connectionElementCollection()
|
Folder |
connectionsRootFolder()
Deprecated.
Deprecated in NX12.0.0. For access to universal connections and folders use
IFEModel.connectionsContainer() .
|
void |
enableFemUpdate()
This method will enable fem update.
|
FluidDomainCollection |
fluidDomains()
Returns the fluid domain collection belonging to this fem part .
|
MeshControlCollection |
meshControls()
Returns the mesh control collection belonging to this fem part .
|
NodeElementManager |
nodeElementMgr()
Returns the node element manager belonging to this fem part .
|
void |
updateFemodel()
This method will update the finite element model so that it
is in sync with any underlying changes.
|
connectionsContainer, feelementLabelMap, fenodeLabelMap, meshManager
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getPdmReferenceAttributeValue, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setPdmReferenceAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
BeamSectionCollection beamSections() throws RemoteException
RemoteException
NodeElementManager nodeElementMgr() throws RemoteException
RemoteException
CAEConnectionCollection caeConnections() throws RemoteException
RemoteException
MeshControlCollection meshControls() throws RemoteException
RemoteException
BoltCollection bolts() throws RemoteException
RemoteException
FluidDomainCollection fluidDomains() throws RemoteException
RemoteException
CfdLocalResolutionConstraintCollection cfdLocalResolutionConstraints() throws RemoteException
RemoteException
CfdContactPreventionConstraintCollection cfdContactPreventionConstraints() throws RemoteException
RemoteException
CfdAutoRefinementConstraintCollection cfdAutoRefinementConstraints() throws RemoteException
RemoteException
CaeReuseLibrary caeReuseLibrary() throws RemoteException
RemoteException
ElementCollection connectionElementCollection() throws RemoteException
RemoteException
void updateFemodel() throws NXException, RemoteException
NXException
RemoteException
void enableFemUpdate() throws NXException, RemoteException
NXException
RemoteException
boolean askUpdatePending() throws NXException, RemoteException
updateFemodel()
to get model up-to-date.
NXException
RemoteException
Folder connectionsRootFolder() throws NXException, RemoteException
IFEModel.connectionsContainer()
.
NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.