Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DieBaseBuilder.DieBaseTypeOpt |
DieBaseBuilder.DieBaseTypeOpt.COMPOUND_DIE
compound die type
|
static DieBaseBuilder.DieBaseTypeOpt |
DieBaseBuilder.DieBaseTypeOpt.DRAW_DIE
draw die type
|
static DieBaseBuilder.DieBaseTypeOpt |
DieBaseBuilder.DieBaseTypeOpt.PDW
progressive die type
|
static DieBaseBuilder.DieBaseTypeOpt |
DieBaseBuilder.DieBaseTypeOpt.SINGLE_DIE
single die type
|
Modifier and Type | Method and Description |
---|---|
DieBaseBuilder.DieBaseTypeOpt |
DieBaseBuilder.dieBaseType()
Returns the die base type( progressive die, single die, draw die or compound die).
|
static DieBaseBuilder.DieBaseTypeOpt |
DieBaseBuilder.DieBaseTypeOpt.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieBaseBuilder.DieBaseTypeOpt |
DieBaseBuilder.DieBaseTypeOpt.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieBaseBuilder.DieBaseTypeOpt[] |
DieBaseBuilder.DieBaseTypeOpt.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieBaseBuilder.setDieBaseType(DieBaseBuilder.DieBaseTypeOpt dieBaseType)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") OR nx_engineering_die_wizard ("NX Engineering Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.