Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static CalculateAreaBuilder.SheetMethodType |
CalculateAreaBuilder.SheetMethodType.CURVE
Using projected curve method to create the sheet body.
|
static CalculateAreaBuilder.SheetMethodType |
CalculateAreaBuilder.SheetMethodType.MESH
Using mesh method to create the sheet body.
|
Modifier and Type | Method and Description |
---|---|
CalculateAreaBuilder.SheetMethodType |
CalculateAreaBuilder.sheetMethod()
Returns the method used to create the projected sheet body.
|
static CalculateAreaBuilder.SheetMethodType |
CalculateAreaBuilder.SheetMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CalculateAreaBuilder.SheetMethodType |
CalculateAreaBuilder.SheetMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CalculateAreaBuilder.SheetMethodType[] |
CalculateAreaBuilder.SheetMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CalculateAreaBuilder.setSheetMethod(CalculateAreaBuilder.SheetMethodType sheetMethod)
License requirements: ug_mold_design ("UG MOLD") OR nx_electrode_wizard ("NX Electrode Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.