public static class CalculateAreaBuilder.SheetMethodType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CURVE
Using projected curve method to create the sheet body.
|
static int |
_MESH
Using mesh method to create the sheet body.
|
static CalculateAreaBuilder.SheetMethodType |
CURVE
Using projected curve method to create the sheet body.
|
static CalculateAreaBuilder.SheetMethodType |
MESH
Using mesh method to create the sheet body.
|
Modifier and Type | Method and Description |
---|---|
static CalculateAreaBuilder.SheetMethodType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CalculateAreaBuilder.SheetMethodType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CalculateAreaBuilder.SheetMethodType[] |
values()
Returns an array that contains the values for this enum.
|
public static final CalculateAreaBuilder.SheetMethodType CURVE
public static final CalculateAreaBuilder.SheetMethodType MESH
public static final int _CURVE
public static final int _MESH
public static CalculateAreaBuilder.SheetMethodType valueOf(int value)
public static CalculateAreaBuilder.SheetMethodType valueOf(String name)
public static CalculateAreaBuilder.SheetMethodType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.