Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static RemoveHolesBuilder.SelectionTypes |
RemoveHolesBuilder.SelectionTypes.BODY
select body type
|
static RemoveHolesBuilder.SelectionTypes |
RemoveHolesBuilder.SelectionTypes.FACE
select face type
|
Modifier and Type | Method and Description |
---|---|
RemoveHolesBuilder.SelectionTypes |
RemoveHolesBuilder.selectionType()
Returns the selection type
License requirements: None. |
static RemoveHolesBuilder.SelectionTypes |
RemoveHolesBuilder.SelectionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RemoveHolesBuilder.SelectionTypes |
RemoveHolesBuilder.SelectionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RemoveHolesBuilder.SelectionTypes[] |
RemoveHolesBuilder.SelectionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RemoveHolesBuilder.setSelectionType(RemoveHolesBuilder.SelectionTypes selType)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.