Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static SpecialPiercingInsertBuilder.PunchOrDieTypes |
SpecialPiercingInsertBuilder.PunchOrDieTypes.DIE |
static SpecialPiercingInsertBuilder.PunchOrDieTypes |
SpecialPiercingInsertBuilder.PunchOrDieTypes.DIE_CAVITY_AND_SLUG_HOLE |
static SpecialPiercingInsertBuilder.PunchOrDieTypes |
SpecialPiercingInsertBuilder.PunchOrDieTypes.PUNCH |
Modifier and Type | Method and Description |
---|---|
SpecialPiercingInsertBuilder.PunchOrDieTypes |
SpecialPiercingInsertBuilder.punchOrDie()
Returns the punch or die
License requirements: None. |
static SpecialPiercingInsertBuilder.PunchOrDieTypes |
SpecialPiercingInsertBuilder.PunchOrDieTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SpecialPiercingInsertBuilder.PunchOrDieTypes |
SpecialPiercingInsertBuilder.PunchOrDieTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SpecialPiercingInsertBuilder.PunchOrDieTypes[] |
SpecialPiercingInsertBuilder.PunchOrDieTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SpecialPiercingInsertBuilder.setPunchOrDie(SpecialPiercingInsertBuilder.PunchOrDieTypes punchOrDie)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.