Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static ClearanceManagementBuilder.Type |
ClearanceManagementBuilder.Type.ASSIGN_CLEARANCES |
static ClearanceManagementBuilder.Type |
ClearanceManagementBuilder.Type.CHECK_CLEARANCES |
Modifier and Type | Method and Description |
---|---|
ClearanceManagementBuilder.Type |
ClearanceManagementBuilder.typeAssignOrCheck()
Returns the clearance management type.
|
static ClearanceManagementBuilder.Type |
ClearanceManagementBuilder.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ClearanceManagementBuilder.Type |
ClearanceManagementBuilder.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ClearanceManagementBuilder.Type[] |
ClearanceManagementBuilder.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ClearanceManagementBuilder.setTypeAssignOrCheck(ClearanceManagementBuilder.Type typeAssignOrCheck)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.