Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static BomListBuilder.BomListTypes |
BomListBuilder.BomListTypes.BOM_LIST
A list includes components in BOM
|
static BomListBuilder.BomListTypes |
BomListBuilder.BomListTypes.HIDE_LIST
A list includes hidden components
|
Modifier and Type | Method and Description |
---|---|
BomListBuilder.BomListTypes |
BomListBuilder.bomListType()
Returns the tree list shows which kind of components should be included in
License requirements: None. |
static BomListBuilder.BomListTypes |
BomListBuilder.BomListTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BomListBuilder.BomListTypes |
BomListBuilder.BomListTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BomListBuilder.BomListTypes[] |
BomListBuilder.BomListTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
int[] |
BomListBuilder.getRows(BomListBuilder.BomListTypes bomListType)
Deprecated.
Deprecated in NX11.0.0. Use
ITableEditorDataProvider.rowCount() instead.
|
void |
BomListBuilder.setBomListType(BomListBuilder.BomListTypes bomListType)
License requirements: ug_mold_design ("UG MOLD") OR nx_electrode_wizard ("NX Electrode Wizard") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.