Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DieInsertBuilder.PositionItems |
DieInsertBuilder.PositionItems.BOTTOM
The position is bottom side
|
static DieInsertBuilder.PositionItems |
DieInsertBuilder.PositionItems.TOP
The position is top side
|
Modifier and Type | Method and Description |
---|---|
DieInsertBuilder.PositionItems |
DieInsertBuilder.position()
Returns the die insert position.
|
static DieInsertBuilder.PositionItems |
DieInsertBuilder.PositionItems.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieInsertBuilder.PositionItems |
DieInsertBuilder.PositionItems.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieInsertBuilder.PositionItems[] |
DieInsertBuilder.PositionItems.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieInsertBuilder.setPosition(DieInsertBuilder.PositionItems position)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.