Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static PunchInsertBuilder.InsertPositionItems |
PunchInsertBuilder.InsertPositionItems.BOTTOM
The position is bottom side
|
static PunchInsertBuilder.InsertPositionItems |
PunchInsertBuilder.InsertPositionItems.TOP
The position is top side
|
Modifier and Type | Method and Description |
---|---|
PunchInsertBuilder.InsertPositionItems |
PunchInsertBuilder.position()
Returns the reverse direction
License requirements: None. |
static PunchInsertBuilder.InsertPositionItems |
PunchInsertBuilder.InsertPositionItems.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PunchInsertBuilder.InsertPositionItems |
PunchInsertBuilder.InsertPositionItems.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PunchInsertBuilder.InsertPositionItems[] |
PunchInsertBuilder.InsertPositionItems.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PunchInsertBuilder.setPosition(PunchInsertBuilder.InsertPositionItems position)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.