Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static CompDrawingBuilder.ComponentTypeSelection |
CompDrawingBuilder.ComponentTypeSelection.ALL
the type of components, read from configuration file
|
Modifier and Type | Method and Description |
---|---|
CompDrawingBuilder.ComponentTypeSelection |
CompDrawingBuilder.componentType()
Returns the component type in mold or die project assembly.
|
static CompDrawingBuilder.ComponentTypeSelection |
CompDrawingBuilder.ComponentTypeSelection.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CompDrawingBuilder.ComponentTypeSelection |
CompDrawingBuilder.ComponentTypeSelection.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CompDrawingBuilder.ComponentTypeSelection[] |
CompDrawingBuilder.ComponentTypeSelection.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CompDrawingBuilder.setComponentType(CompDrawingBuilder.ComponentTypeSelection componentType)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.