Interface | Description |
---|---|
AccessorEvaluatorBuilder |
Evaluates an object based on a property value or an index
To create a new instance of this class, use AMEManager.createAccessorEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
AMEBaseBuilder |
JA class for the insert Eng object dialog
This is an abstract class, and cannot be instantiated. |
AMEBaseNode |
Represents Base Node
Use the static method in this class to obtain an instance. |
AmeDebugSession |
Represents a class that is used for AME testing.
|
AMEEngineeringObjectLabel |
Represents Engineering Object Label Object
This object does not need a creator. |
AMEEngObject |
Represents Engineering Object
This object does not need a creator. |
AMEExtendedObject |
Represents Extended Object
Use the static method in this class to obtain an instance. |
AMEGroup |
Group Journaling class
This object does not need a creator. |
AMEGroupFolder |
Group Folder Journaling class
This object does not need a creator. |
AMEManager |
Represents a manager of automation designer objects
To obtain an instance of this class, refer to Session Created in NX11.0.0 |
AMENamingRule |
Represents Naming Rule Object
This object does not need a creator. |
AMEPlcHwItem |
Represents Plc Hw Item
Use the static method in this class to obtain an instance. |
AMEPort |
Represents Port
Use the static method in this class to obtain an instance. |
AMEQuery |
The Query Object
This is an abstract class, and cannot be instantiated. |
AMEQueryGroup |
The Query Group
This is an abstract class, and cannot be instantiated. |
AMEReportRule |
Represents Report Rule Object
This object does not need a creator. |
AncestorEvaluatorBuilder |
Evaluates an ancestor for a given aspect and a starting point
To create a new instance of this class, use AMEManager.createAncestorEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
ApplicationBuilder |
Create the AD application builder see AMEApplicationBuilder
To create a new instance of this class, use AMEManager.createApplicationBuilder(nxopen.Part) Created in NX11.0.0 |
AspectDetailsBuilder |
JA Class for the Aspect Details UI Block
This object does not need a creator. |
AspectNavigatorPreferencesBuilder |
JA class for aspect navigator builder
To create a new instance of this class, use AMEManager.createAspectNavigatorPreferencesBuilder(nxopen.Part) Created in NX11.0.0 |
AspectNode |
Aspect Node Journaling class
This object does not need a creator. |
AspectPrefixBuilder |
represents the builder class which is used to define Aspect Prefixes and Delimiter for
Project To create a new instance of this class, use AMEManager.createAspectPrefixBuilder(nxopen.Part) Created in NX11.0.0 |
AspectRoot |
AspectRoot Node Journaling class
This object does not need a creator. |
AssignAspectBuilder |
Reassign a single aspect of an Engineering Object
To create a new instance of this class, use AMEManager.createAssignAspectBuilder(nxopen.Part) Created in NX11.0.0 |
AssignmentPort |
Represents AssignmentPort
Use the static method in this class to obtain an instance. |
AssignSubnetBuilder |
Reassign a single aspect of an Engineering Object
To create a new instance of this class, use AMEManager.createAssignSubnetBuilder(nxopen.Part) Created in NX12.0.0 |
AssignTemplateToProductBuilder |
Builder class to assign a template object to
ProductDefinition To create a new instance of this class, use AMEManager.createAssignTemplateToProductBuilder(nxopen.ame.ProductDefinition) Created in NX12.0.0 |
AssignTypeBuilder |
Builder for selecting an engineering object definition
To create a new instance of this class, use AMEManager.createAssignTypeBuilder(nxopen.Part) Created in NX12.0.0 |
AttributeHolder |
JA class for the AttributeHolder object
This is an abstract class, and cannot be instantiated. |
BaseDefinitionAttributeHolder |
BaseDefinition Atributes Holder Object
This does not need a creator. |
BaseEvaluatorBuilder |
Represents the builder for all the evaluators.
|
BasicPropertiesBuilder |
Represents a re-usable component for basic properties such as name and description
This object does not need a creator. |
BreakTemplateBuilder |
JA class for the insert Eng object dialog
To create a new instance of this class, use AMEManager.createBreakTemplateBuilder(nxopen.Part, nxopen.ame.AMEEngObject) Created in NX11.0.0 |
BulkConnectionBuilder |
builder for the bulk connection dialog
To create a new instance of this class, use AMEManager.createBulkConnectionBuilder(nxopen.Part) Created in NX11.0.0 |
BulkEngineeringObjectBuilder |
BulkEngineeringObjectBuilder class will be used for bulk Engineering Object Operation.
|
CabinetComponentNode |
Cabinet Component Node class
This object does not need a creator. |
CabinetDesignBuilder |
the builder for creating cabinet design
To create a new instance of this class, use AMEManager.createCabinetDesignBuilder(nxopen.Part) Created in NX12.0.0 |
CabinetNode |
Cabinet Node class
This object does not need a creator. |
CabinetObject |
Cabinet Object class
This object does not need a creator. |
CabinetRoot |
Cabinet Root Node class
This object does not need a creator. |
CallMethodRuleBuilder |
JA class for the call method rule dialog
To create a new instance of this class, use AMEManager.createCallMethodRuleBuilder(nxopen.Part, nxopen.ame.PlcCodePosition, nxopen.ame.PlcBlock, nxopen.ame.PlcRule.Type, nxopen.ame.PlcRule.RefObjectType, nxopen.ame.PlcRule.ReplacementType, int, int, int) Created in NX12.0.0 |
ChildrenEvaluatorBuilder |
Evaluates the children objects for a given aspect and a starting point
To create a new instance of this class, use AMEManager.createChildrenEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
ConditionsBuilder |
JA class for the conditions dialog .
|
ConfigureResultTableBuilder |
Represents configure result table class builder
To create a new instance of this class, use AMEManager.createConfigureResultTableBuilder(nxopen.ame.AMEQuery) Created in NX12.0.0 |
ConnectedObjectsEvaluatorBuilder |
Evaluates the connected objects for the given port and a starting point
To create a new instance of this class, use AMEManager.createConnectedObjectsEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
ConnectToLibraryItemBuilder |
JA class for the connect to library item dialog
To create a new instance of this class, use AMEManager.connectToLibraryItemBuilder(nxopen.Part, nxopen.ame.InterfaceMemberPort) Created in NX11.0.0 |
CreateDefinitionBuilder |
Create and classify definition
This object does not need a creator. |
CreateEngObjectDefinitionBuilder |
Create and classify engineering object definition
To create a new instance of this class, use AMEManager.createEngObjectDefinitionBuilder(nxopen.Part) Created in NX11.0.0 |
CreatePmiNoteBuilder |
Create PMINote dialog JA class
To create a new instance of this class, use AMEManager.createPmiNoteBuilder(nxopen.Part) Created in NX11.0.0 |
CreateProductBuilder |
Create and classify product
To create a new instance of this class, use AMEManager.createProductBuilder(nxopen.Part) Created in NX11.0.0 |
CreateTemplateBuilder |
Create Template dialog JA class
To create a new instance of this class, use AMEManager.createTemplateBuilder(nxopen.Part) Created in NX11.0.0 |
CreateTemplateDefinitionBuilder |
Create and classify template definition
To create a new instance of this class, use AMEManager.createTemplateDefinitionBuilder(nxopen.Part) Created in NX11.0.0 |
DefineAspectBuilder |
Define Aspects for Engineering Object Definition
To create a new instance of this class, use AMEManager.defineAspectBuilder(nxopen.Part) Created in NX11.0.0 |
DeviceFunctionDef |
Device Function Def class
This object does not need a creator. |
DiagramManager |
Represents an object that manages sheet elements.
|
DocumentRoot |
Document Root Node class
This object does not need a creator. |
DocumentStructureBuilder |
Class to define Document Structure
To create a new instance of this class, use AMEManager.createDocumentStructureBuilder(nxopen.Part) Created in NX11.0.0 |
EClassClassNode |
EClassData Tree Node class
This object does not need a creator. |
EClassDataRoot |
EClassData Root Node class
This object does not need a creator. |
EClassFolderNode |
EClass Folder Node class
This object does not need a creator. |
EClassNode |
EClassData Tree Node class
This object does not need a creator. |
EClassObjectNode |
EClassData Tree Node class
This object does not need a creator. |
EClassSegmentNode |
EClass Segment Node class
This object does not need a creator. |
EClassVersionNode |
EClass Version Node class
This object does not need a creator. |
EditAnnotationBuilder |
the builder for creating edit annotation
To create a new instance of this class, use AMEManager.createEditAnnotationBuilder(nxopen.Part, nxopen.ame.AMEExtendedObject) Created in NX12.0.0 |
EditClauseBuilder |
Naming Rule Builder
To create a new instance of this class, use AMEManager.createEditClauseBuilder(nxopen.Part, nxopen.ame.AMEQuery, nxopen.ame.QueryClause) Default values. |
EditEngineeringObjectBuilder |
JA class for the Eng object dialog
To create a new instance of this class, use AMEManager.createEditEngineeringObjectBuilder(nxopen.Part, nxopen.ame.AMEEngObject) Created in NX11.0.0 |
EditOrderBuilder |
JA class for the Edit Order dialog
To create a new instance of this class, use AMEManager.createEditOrderBuilder(nxopen.Part, nxopen.NXObject) Created in NX12.0.0 |
EditQueryBuilder |
Edit Query Builder
To create a new instance of this class, use AMEManager.createEditQueryBuilder(nxopen.Part) Created in NX11.0.0 |
ElectricalAnnotationSettingsBuilder |
JA class for the Electrical Annotation Settings dialog
To create a new instance of this class, use AMEManager.createElectricalAnnotationSettingsBuilder(nxopen.Part) Created in NX11.0.0 |
ElectricalConnectionSettingsBuilder |
Builder object for changing electrical connection settings on diagramming pages associated with the
Project . |
EngineeringObjectAspectDetailBuilder |
JA class for the Engineering Object Aspect Detail UI block
.
|
EngineeringObjectBaseBuilder |
JA class for the insert Eng object dialog
This is an abstract class, and cannot be instantiated. |
EngineeringObjectBuilder |
JA class for the insert Eng object dialog
To create a new instance of this class, use AMEManager.createEngineeringObjectBuilder(nxopen.Part) Created in NX11.0.0 |
EngineeringObjectDefinitionLabelBuilder |
JA class for the insert Engineering object definition label dialog
To create a new instance of this class, use AMEManager.createEngineeringObjectDefinitionLabelBuilder(nxopen.Part) Created in NX11.0.0 |
EngineeringObjectNameBuilder |
JA class for the Engineering Object and Engineering Object def name and description superclass UI block
.
|
EOAttributeHolder |
EOAttributeHolder Atributes Holder Object
This does not need a creator. |
EODataItemAttributeHolder |
EODef Atributes Holder Object
This does not need a creator. |
EODefAttributeHolder |
EODef Atributes Holder Object
This does not need a creator. |
EplanImportProjectTemplateBuilder |
EplanImportProjectTemplateBuilder
To create a new instance of this class, use AMEManager.createEplanImportProjectTemplateBuilder(nxopen.Part) Created in NX12.0.0 |
EPLANPlug |
Represents EPLANPlug
Use the static method in this class to obtain an instance. |
EplanProjectGenerationBuilder |
the eplan project generation dialog builder
To create a new instance of this class, use AMEManager.createEplanProjectGenerationBuilder(nxopen.Part) Default values. |
EPLANProjectSettings |
Eplan project settings Node Journaling class
To create or edit an instance of this class, use EplanSettingsBuilder Created in NX11.0.0 |
EplanProjectTemplateAndStructureBuilder |
JA class for the Eplan project template dialog
To create a new instance of this class, use AMEManager.createEplanProjectTemplateAndStructureBuilder(nxopen.Part) Created in NX12.0.0 |
EplanSettingsBuilder |
EplanSettingsBuilder
To create a new instance of this class, use AMEManager.createEplanSettingsBuilder(nxopen.Part, nxopen.ame.AMEBaseNode) Created in NX11.0.0 |
EPLANSocket |
Represents EPLANSocket
Use the static method in this class to obtain an instance. |
EplanStructureIdentifierOrderBuilder |
Represents a Eplan Structure identifier order Builder
To create a new instance of this class, use AMEManager.createEplanStructureIdentifierOrderBuilder(nxopen.Part) Created in NX12.0.0 |
EplanStructureSettings |
Eplan structure settings Journaling class
Will be added once available . |
EvaluatorCopyToBuilder |
Copies evaluator and its dependents from one engineering object to another
To create a new instance of this class, use AMEManager.createEvaluatorCopyToBuilder(nxopen.Part) Created in NX12.0.0 |
ExportEClassMappingBuilder |
Export eclass mapping into file
To create a new instance of this class, use AMEManager.createExportEclassMappingBuilder(nxopen.Part) Created in NX12.0.0 |
ExpressionEvaluator |
Represents an Expression Evaluator
This object does not need a creator. |
ExtractAttribute |
Extract Attribute Journaling class
This object does not need a creator. |
ExtractAttributeAbsoluteBuilder |
Create a extract attribute
This object does not need a creator. |
ExtractAttributeBaseBuilder |
Create a extract attribute
This is an abstract class, and cannot be instantiated. |
ExtractAttributeBuilder |
Create a extract attribute
To create a new instance of this class, use AMEManager.createExtractAttributeBuilder(nxopen.Part) Created in NX11.0.0 |
ExtractAttributeCurrentObjectBuilder |
Create a extract attribute
This object does not need a creator. |
ExtractAttributePortBuilder |
Create a extract port attribute builder
This object does not need a creator. |
ExtractAttributeRelativeBuilder |
Create a extract attribute
This object does not need a creator. |
FormSheetBuilder |
JA class for the Form Sheet dialog
To create a new instance of this class, use AMEManager.createFormSheetBuilder(nxopen.Part, nxopen.ame.FormSheetObject) Default values. |
FormSheetObject |
JA class for the FormSheetObject
This is an abstract class, and cannot be instantiated. |
FormSheetSettingsBuilder |
JA class for the Form Sheet Settings dialog
To create a new instance of this class, use AMEManager.createFormSheetSettingsBuilder(nxopen.Part) Created in NX12.0.0 |
FragmentAttributeHolder |
Fragment Object Atributes Holder
This does not need a creator. |
FragmentBuilder |
Represents a Fragment creation class Builder
To create a new instance of this class, use AMEManager.createFragmentBuilder(nxopen.Part) Created in NX11.0.0 |
FragmentObject |
Represents a Fragment Object
This object does not need a creator. |
FunctionCallInstanceBuilder |
JA class for the reuse rule dialog
To create a new instance of this class, use AMEManager.createFunctionCallInstanceBuilder(nxopen.Part, nxopen.ame.PlcBlock) Created in NX12.0.0 |
GeneralAnnotationSettingsBuilder |
builder for the general annotation settings dialog
To create a new instance of this class, use AMEManager.createGeneralAnnotationSettingsBuilder(nxopen.Part) Created in NX11.0.0 |
GeneralConnectionSettingsBuilder |
Builder for the General Connection Settings dialog
To create a new instance of this class, use AMEManager.createGeneralConnectionSettingsBuilder(nxopen.Part) Created in NX11.0.0 |
GenerateReportsBuilder |
Comment
To create a new instance of this class, use AMEManager.createGenerateReportsBuilder(nxopen.Part) Created in NX11.0.0 |
GlobalSelectionBuilder |
GlobalSelectionBuilder
To create a new instance of this class, use AMEManager.createGlobalSelectionBuilder(nxopen.Part) Created in NX11.0.0 |
GroupBuilder |
JA class for groups
To create a new instance of this class, use AMEManager.createGroupBuilder(nxopen.Part, nxopen.ame.AMEGroup) Created in NX11.0.0 |
GroupRoot |
Group Root Node Journaling class
This object does not need a creator. |
IEngObject |
Represents Engineering Object .
|
ImportEClassMappingBuilder |
Import eClass mapping
To create a new instance of this class, use AMEManager.createImportEclassMappingBuilder(nxopen.Part) Created in NX12.0.0 |
ImportEClassProductBuilder |
Imports a eclass product xml file
To create a new instance of this class, use AMEManager.createImportEclassProductBuilder(nxopen.Part) Created in NX12.0.0 |
ImportEClassSchemaBuilder |
Imports a eclass schema xml file
To create a new instance of this class, use AMEManager.createImportEclassSchemaBuilder(nxopen.Part) Created in NX12.0.0 |
ImportEplanPageMacroBuilder |
ImportEplanPageMacroBuilder
To create a new instance of this class, use AMEManager.createImportEplanPageMacroBuilder(nxopen.Part) Created in NX11.0.0 |
ImportGlobalMappingBuilder |
Imports a global mapping xml file
To create a new instance of this class, use AMEManager.createImportGlobalMappingBuilder(nxopen.Part) Created in NX12.0.0 |
ImportHWXmlBuilder |
the Import HW Xml builder
To create a new instance of this class, use AMEManager.createImportHwxmlBuilder(nxopen.Part, nxopen.ame.AMEBaseNode) Created in NX11.0.0 |
ImportNode |
Import Object Journaling class
This object does not need a creator. |
ImportObject |
Import Object Journaling class
This object does not need a creator. |
InsertObjectBuilder |
JA class for Insert Object dialog
To create a new instance of this class, use AMEManager.createInsertObjectBuilder(nxopen.Part) Created in NX12.0.0 |
InsertSettingsBuilder |
Re-usable UI for Settings properties in Insert EO and Insert Template dialog .
|
InstanceDataBlockBuilder |
JA class for the reuse rule dialog
To create a new instance of this class, use AMEManager.createInstanceDataBlockBuilder(nxopen.Part, nxopen.ame.PlcBlock, nxopen.ame.InstanceDataBlockBuilder.CreateMode) Created in NX11.0.0 |
InstantiateBaseDefinitionReuseSelectionBuilder |
Builder for selecting base definition
this is a block . |
InstantiateTemplateBulkBuilder |
JA class for the insert Eng object dialog
To create a new instance of this class, use AMEManager.createInstantiateTemplateBulkBuilder(nxopen.Part, java.lang.String) Default values. |
InterfaceMemberPort |
InterfaceMemberPort Journaling class
This object does not need a creator. |
InterruptionPointBuilder |
Represents builder for AME::DB::InterruptionPoint
To create a new instance of this class, use AMEManager.createInterruptionPointBuilder(nxopen.Part, nxopen.ame.AMEExtendedObject) Created in NX12.0.0 |
IPort |
Represents an IPort
This is an abstract class, and cannot be instantiated. |
IPortsContainer |
Represents Ports Container .
|
LayoutDefinitionBuilder |
interface for the LayoutDefinitionBuilder
To create a new instance of this class, use AMEManager.createLayoutDefinitionBuilder(nxopen.Part) Created in NX11.0.0 |
LDCachedAttribute |
JA class for the Line Design cache Attribute object
This is an abstract class, and cannot be instantiated. |
LineDesignerMappingBuilder |
Line Designer mapping dialog JA interface
To create a new instance of this class, use AMEManager.createLineDesignerMappingBuilder(nxopen.Part) Default values. |
LinkSymbolToDeviceTypeBuilder |
JA class for LinkSymbolToDeviceTypeBuilder dialog
To create a new instance of this class, use AMEManager.createLinkSymbolToDeviceTypeBuilder(nxopen.Part) Created in NX11.0.0 |
LoadLineDesignerBuilder |
JA class for the insert LoadLineDesigner dialog
To create a new instance of this class, use AMEManager.createLoadLineDesignerBuilder(nxopen.Part) Created in NX11.0.0 |
Manage2dSymbolsBuilder |
Represents a Manage2dSymbolsBuilder class Builder
To create a new instance of this class, use AMEManager.createManage2dSymbolsBuilder(nxopen.Part) Default values. |
Manage3DModelsBuilder |
Represents the builder that is used to assign 3D models to a
ProductDefinition
To create a new instance of this class, use AMEManager.createManage3dmodelsBuilder(nxopen.Part) Created in NX11.0.0 |
ManageEclassMappingBuilder |
Represents a ManageEclassMappingBuilder class Builder
To create a new instance of this class, use AMEManager.createManageEclassmappingBuilder(nxopen.Part) Created in NX11.0.0 |
ManageObjectTypeBuilder |
Builder class for assigning AD type to
Part and name to Component To create a new instance of this class, use AMEManager.createManageObjectTypeBuilder(nxopen.Part) Created in NX12.0.0 |
MapToExistingObjectBuilder |
Line Designer map to existing (EO) dialog JA interface
To create a new instance of this class, use AMEManager.createMapToExistingObjectBuilder(nxopen.Part) Created in NX11.0.0 |
MountingInterface |
Represents a Mounting Interface
This object does not need a creator. |
MountingInterfaceBuilder |
Builder class for creating mounting interface object in
Part To create a new instance of this class, use AMEManager.createMountingInterfaceBuilder(nxopen.Part) Default values. |
MultipleObjectsBuilder |
JA class for the insert Eng object dialog
This is an abstract class, and cannot be instantiated. |
MultiValueObjectsPort |
MultiValueObjectsPort Journaling class
This object does not need a creator. |
NamingRuleBuilder |
Naming Rule Builder
To create a new instance of this class, use NamingRuleListBuilder.createRule() Created in NX11.0.0 |
NamingRuleBuilderList |
Represents a list of objects.
|
NamingRuleListBuilder |
Classification to Engineering Object Name Map Builder
this is a block . |
NamingRuleSettingsBuilder |
JA class for dialog for naming rule settings
To create a new instance of this class, use AMEManager.createNamingRuleSettingsBuilder(nxopen.Part) Created in NX11.0.0 |
ObjectConnectionBuilder |
JA class for the reuse object connection block .
|
ObjectConnectionDetailBuilder |
JA class for the reuse object connection detail block .
|
ObjectEvaluatorBuilder |
Evaluates the object given a starting point
To create a new instance of this class, use AMEManager.createObjectEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
ObjectNameBuilder |
Object Name JA class .
|
ObjectNameIndexBuilder |
Object Name Index JA class .
|
OperandRuleBuilder |
JA class for the parameter rule dialog
To create a new instance of this class, use AMEManager.createOperandRuleBuilder(nxopen.Part, nxopen.ame.PlcCodePosition, nxopen.ame.PlcBlock, int, int, nxopen.ame.PlcRule.Type) Created in NX11.0.0 |
OperatorRuleBuilder |
OperatorRule Dialog
To create a new instance of this class, use AMEManager.createOperatorRuleBuilder(nxopen.Part, nxopen.ame.PlcCodePosition, nxopen.ame.PlcBlock, nxopen.ame.PlcRule.Type, nxopen.ame.PlcRule.RefObjectType, nxopen.ame.PlcRule.ReplacementType, int, int, int) Created in NX12.0.0 |
OpticalAnnotationSettingsBuilder |
JA class for the Optical Annotation Settings dialog
To create a new instance of this class, use AMEManager.createOpticalAnnotationSettingsBuilder(nxopen.Part) Created in NX12.0.0 |
OpticalConnectionSettingsBuilder |
Builder object for changing optical connection settings on diagramming pages associated with the
Project To create a new instance of this class, use AMEManager.createOpticalConnectionSettingsBuilder(nxopen.Part) Created in NX12.0.0 |
OrderAspectsBuilder |
Represents a
OrderAspectsBuilder for changing the order of Navigator
To create a new instance of this class, use AMEManager.createOrderAspectsBuilder(nxopen.Part) Created in NX11.0.0 |
PageAttributeHolder |
Page Object Atributes Holder
This does not need a creator. |
PageBuilder |
Represents a Page creation class Builder
To create a new instance of this class, use AMEManager.createPageBuilder(nxopen.Part) Default values. |
PageNamingBuilder |
Class to define Page naming schema
To create a new instance of this class, use AMEManager.createPageNamingBuilder(nxopen.Part) Default values. |
PageNode |
Represents a Page Node
This object can not be created directly. |
PageObject |
Represents a Page Object
This object does not need a creator. |
ParameterRuleBuilder |
JA class for the parameter rule dialog
To create a new instance of this class, use AMEManager.createParameterRuleBuilder(nxopen.Part, nxopen.ame.MultiValueObjectsPort, nxopen.ame.PlcRule.Type, nxopen.ame.MultiValueObjectsPort.JaAmeValueObjectUsageType) Created in NX12.0.0 |
ParentEvaluatorBuilder |
Evaluates the parent object for a given aspect and a starting point
To create a new instance of this class, use AMEManager.createParentEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
PlaceAutomationBuilder |
Reassign a single aspect of an Engineering Object
To create a new instance of this class, use AMEManager.createPlaceAutomationBuilder(nxopen.Part) Created in NX12.0.0 |
PlcBlock |
Plc Block Node Journaling class
This is an abstract class. |
PlcCodePosition |
Represents Plc Code Position Object
This object does not need a creator. |
PlcMemoryAreaBuilder |
Represents a Subnet creation class Builder
To create a new instance of this class, use AMEManager.createPlcMemoryAreaBuilder(nxopen.Part, nxopen.ame.AMEBaseNode) Created in NX12.0.0 |
PlcMethod |
Plc Method Node Journaling class
This is an abstract class. |
PlcMethodBuilder |
The Journalling class for PlcMethodBuilder
To create a new instance of this class, use AMEManager.createPlcMethodBuilder(nxopen.Part, nxopen.ame.PlcMethod) Created in NX11.0.0 |
PlcRule |
PlcRule Journaling class
This object does not need a creator. |
PlcSoftwareGenPort |
PlcSoftwareGenPort Journaling class
This object does not need a creator. |
PlcSymbolBuilder |
Class to create Functional Tags and assign them to PLC Channels
To create a new instance of this class, use AMEManager.createPlcSymbolBuilder(nxopen.Part, nxopen.ame.AMEBaseNode) Created in NX11.0.0 |
PlcSymbolsEvaluatorBuilder |
Evaluates the PLC tags for a given aspect and a starting point
To create a new instance of this class, use AMEManager.createPlcSymbolsEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
PlcVendorSymbolBuilder |
Represents a Subnet creation class Builder
To create a new instance of this class, use AMEManager.createPlcVendorSymbolBuilder(nxopen.Part, nxopen.NXObject) Created in NX12.0.0 |
PortArtifact |
Represents a base class that provides common methods for port artifact in a
ConditionalElementRevision . |
PortAttributeHolder |
Port Object Atributes Holder
This does not need a creator. |
PortBuilder |
builder for the software block properties dialog
To create a new instance of this class, use AMEManager.createPortBuilder(nxopen.Part, nxopen.NXObject, nxopen.NXObject) Created in NX11.0.0 |
PortConnectionBuilder |
builder for the port connector dialog
To create a new instance of this class, use AMEManager.createPortConnectionBuilder(nxopen.Part, nxopen.NXObject) Created in NX11.0.0 |
PortEvaluatorBuilder |
Evaluates the port objects for the given port and a starting point
To create a new instance of this class, use AMEManager.createPortEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
PortsManagerBuilder |
Provides journal methods for the ports manager dialog.
|
ProductComponent |
Product Component class
This object does not need a creator. |
ProductComponentInstance |
Product Component Instance class
This object does not need a creator. |
ProductDefAttributeHolder |
ProductDefinition Atributes Holder Object
This does not need a creator. |
ProductDefinition |
JA class for the Product Definition object
This is an abstract class, and cannot be instantiated. |
ProductDefinitionRoot |
Product Definition Root class
This object does not need a creator. |
ProductMatchingRulesBuilder |
Represents Product Matching Rules class builder
To create a new instance of this class, use AMEManager.createProductMatchingRulesBuilder(nxopen.Part) Created in NX11.0.0 |
ProductSelectionBuilder |
JA class for Product Selection dialog
To create a new instance of this class, use AMEManager.createProductSelectionBuilder(nxopen.Part) Default values. |
ProductSelectionDetailsBuilder |
Represents a Product Selection Details class Builder
To create a new instance of this class, use AMEManager.createProductSelectionDetailsBuilder(nxopen.Part) Created in NX11.0.0 |
Project |
Project Journaling class
Created by Application_AME_ApplicationBuilder when we enter the application . |
ProjectEngineeringObjectBuilder |
JA class for the insert Project Eng object dialog
To create a new instance of this class, use AMEManager.createProjectEngineeringObjectBuilder(nxopen.Part) Created in NX11.0.0 |
PropertyEvaluatorBuilder |
Evaluates the property of an object given a category and property
To create a new instance of this class, use AMEManager.createPropertyEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
QueryBuilder |
Represents query class builder
To create a new instance of this class, use AMEManager.createQueryBuilder(nxopen.Part) Created in NX11.0.0 |
QueryClause |
JA class for the QueryClause object
This is an abstract class, and cannot be instantiated. |
QueryFolder |
Query Folder Journaling class
This object does not need a creator. |
QueryNode |
The Query Node
This is an abstract class, and cannot be instantiated. |
ReferenceDesignationSetNode |
Reference Designation Set Node Journaling class
This object does not need a creator. |
ReferenceObjectBuilder |
Re-usable UI consist of a context and source selection .
|
ReportsSettingsBuilder |
interface for the ReportsSettingsBuilder
To create a new instance of this class, use AMEManager.createReportsSettingsBuilder(nxopen.Part) Created in NX11.0.0 |
ReportTemplateBuilder |
Class to create Report Template and assign the ReportQuery and Report Layout to them
To create a new instance of this class, use AMEManager.createReportTemplateBuilder(nxopen.Part) Created in NX11.0.0 |
SaveToLibraryBuilder |
Create Software Block JA class
To create a new instance of this class, use AMEManager.createSaveToLibraryBuilder(nxopen.Part) Created in NX11.0.0 |
SchematicSymbol |
Represents a Schematic Symbol object
This object does not need a creator. |
SchematicSymbolConfigurationBuilder |
JA class for SchematicSymbolConfigurationBuilder dialog
To create a new instance of this class, use AMEManager.createSchematicSymbolConfigurationBuilder(nxopen.Part) Created in NX11.0.0 |
SelectAMEBaseNode |
Represents a single object selection.
|
SelectAMEBaseNodeList |
Represents a list of objects on a selection list.
|
SelectAMEExtendedObject |
Represents a single object selection.
|
SelectAMEPort |
Represents a single object selection.
|
SelectAndHighlightBuilder |
Represents a
SelectAndHighlightBuilder for select and highlight in the Navigators
To create a new instance of this class, use AMEManager.selectAndHighlightBuilder(nxopen.Part) Created in NX11.0.0 |
SelectAspectNode |
Represents a single object selection.
|
SelectBaseDefinitionNodeBuilder |
Builder for selecting base definition node from navigators
This object does not need a creator . |
SelectClassificationBuilder |
Select a part from the reuse library .
|
SelectClassificationFromTreeBuilder |
Select Type from the Classification Library
This object does not need a creator. |
SelectionBaseDefinitionBuilder |
Journalling Interface class for Builder which allows selection of BaseDefinition.
|
SelectionEngineeringObjectDefinitionBuilder |
JA class for the Engineering Object Definition Block
This object does not need a creator. |
SelectMountingInterfaceLocationBuilder |
Builder for selecting mounting interface location from graphics window
This object does not need a creator . |
SelectProductDefinitionBuilder |
JA class for the Product Definition Selection
This object does not need a creator. |
SelectProductOrEoDefinitionBuilder |
JA class for the Product Definition or Engineering Object Definition Selection
This object does not need a creator. |
ShowHideObjectsBuilder |
JA class for ShowHideObjectsBuilder
To create a new instance of this class, use AMEManager.createShowHideObjectsBuilder(nxopen.Part) Created in NX11.0.0 |
Snap3DModelsBuilder |
Represents a Snap3DModelsBuilder class Builder
To create a new instance of this class, use AMEManager.createSnap3dmodelsBuilder(nxopen.Part) Created in NX12.0.0 |
SortingBlockBuilder |
Sorts the list expression output according to the property .
|
SubnetBuilder |
Represents a Subnet creation class Builder
To create a new instance of this class, use AMEManager.createSubnetBuilder(nxopen.Part) Created in NX12.0.0 |
SWStatusItem |
Represents SW Status Item
. |
SymbolAnnotationBuilder |
Represents a Symbol Annotation creation class Builder
To create a new instance of this class, use AMEManager.createSymbolAnnotationBuilder(nxopen.Part) Created in NX12.0.0 |
SymbolAnnotationSettingsBuilder |
JA class for the symbol settings
To create a new instance of this class, use AMEManager.createSymbolAnnotationSettingsBuilder(nxopen.Part) Created in NX12.0.0 |
SymbolAuthoringBuilder |
Represents a Symbol Authoring class Builder
To create a new instance of this class, use AMEManager.createSymbolAuthoringBuilder(nxopen.Part) Default values. |
SymbolRoot |
Symbol Root Node class
This object does not need a creator. |
TCSavedQueriesBuilder |
Represents a TC Saved Queries builder
To create a new instance of this class, use AMEManager.createEditQueryScopeBuilder(nxopen.Part, nxopen.ame.AMEQuery, nxopen.ame.QueryClause) Created in NX11.0.0 |
TeeJunctionBuilder |
JA class for creating Tee Junction
To create a new instance of this class, use AMEManager.createTeeJunctionBuilder(nxopen.Part) Created in NX12.0.0 |
TiaPortalProjectSettings |
Tia Portal project settings node journaling class
This object does not need a creator. |
TiaPortalProjectSettingsBuilder |
TiaPortalProjectSettingsBuilder
To create a new instance of this class, use AMEManager.createTiaPortalProjectSettingsBuilder(nxopen.Part) Created in NX12.0.0 |
TiaProjectItemBuilder |
the TIA project item builder
To create a new instance of this class, use AMEManager.createTiaprojectItemBuilder(nxopen.Part) Created in NX11.0.0 |
TransferFileDataBuilder |
Imports a new one or updates the existing configuration in AD Upstream Data Navigator from the external file.
|
TypeMappingBuilder |
JA class for the type mapping dialog
this is a block . |
TypeMappingBuilderList |
Represents a list of objects.
|
TypeMappingListBuilder |
Type Mapping List Builder
To create a new instance of this class, use AMEManager.createTypeMappingListBuilder(nxopen.Part) Created in NX11.0.0 |
UnloadLineDesignerBuilder |
JA class for the insert UnloadLineDesigner dialog
To create a new instance of this class, use AMEManager.createUnloadLineDesignerBuilder(nxopen.Part) Created in NX11.0.0 |
UpstreamDataRoot |
UpstreamData Root Node class
This object does not need a creator. |
Class | Description |
---|---|
AccessorEvaluatorBuilder.AccessType |
Choices for access type either by an index or property
|
AccessorEvaluatorBuilder.PositionTypeValue |
Choices for position to be either begin, end or defined by index
|
AddressObjectIotype |
Definition of the Address Object I/O types
See Xml node IoType
|
AMEBaseNode.NodeType |
Define the node type
|
AmeDebugSession.NavigatorType |
Represents type of the navigator
|
AmeDebugSession.ObjectType |
Represents type of the object
|
AmeDebugSessionFactory | |
AmeElectricalConnectionPotentialType |
Represents electrical connection Pontential Types
|
AmeJunctionRepresentationStyleType |
Representation style for Tee Junction.
|
AMEManager.CreateStationType |
Type of PLC Station
|
AMEManager.DeleteType |
the deletion type
|
AMEManager.PasteObjectsData |
This class holds the data returned from
AMEManager.pasteObjects(nxopen.ame.AMEBaseNode) |
AMEManager.PasteStatus |
the status of paste operation
|
AMEManagerFactory | |
AmeOpticalConnectionFiberType |
Represents optical connection fiber types
|
AmeTeeJunctionType |
Represents the type of TeeJunction
|
AmeTeeJunctionVariant |
Represents Tee Junction variant index
|
AncestorEvaluatorBuilder.JaAspectEvaluatorBuilderNavCriteria |
Choices for navigation criteria - Could be By Levels or By Property
|
AncestorEvaluatorBuilder.JaAspectEvaluatorBuilderNavDirection |
Choices for direction of navigation - Could be from starting object upwards, or from root node downwards
|
AspectPrefixBuilder.DelimiterType |
represents delimiter type
|
BaseEvaluatorBuilder.ConditionType |
choices for condition type filter for navigations that return a list of filtered objects
|
BaseEvaluatorBuilder.ContextType |
choices for aspect context type, can either be function, location, product, or automation
|
BusInterfaceType |
Bus Interface type.
|
CabinetRoot.CabinetState |
Represents cabinet state
|
CallMethodRuleBuilder.CreationType |
replace or insert rule Type
|
ChildrenEvaluatorBuilder.FilterType |
choices for object type filter, can either be local modules, program blocks, plc data types, or tags
|
ConstantType |
The Plc Constant types
|
DiagramManagerFactory | |
DocumentType |
Represents the type of document
|
EditClauseBuilder.Operator |
the query operator
|
EditClauseBuilder.QueryClauseOperatorType |
the clause operator
|
EditClauseBuilder.Types |
the type of object to be used for edit clause
|
EditEngineeringObjectBuilder.SourceType |
Assign EOs or POUs
|
ElectricalAnnotationSettingsBuilder.AnnotationAttrType |
Represents the type of annotations
|
EngineeringObjectAspectDetailBuilder.Columns |
Aspect Detail columns
|
EngineeringObjectAspectDetailBuilder.NameSource |
Aspect name from
|
ExtractAttributeBuilder.Type |
extract type Type
|
FormSheetBuilder.SizeOption |
Represents form sheet size option
|
FormSheetBuilder.StandardMetricSize |
Represents standard metric sizes for form sheet
|
GeneralAnnotationSettingsBuilder.AnnotationSeparator |
the separator for annotation set
|
GeneralAnnotationSettingsBuilder.HorizontalTextPosition |
horizontal text postion type
|
GeneralAnnotationSettingsBuilder.SourceAndTargetSeparator |
the separator between Source and Target
|
GeneralAnnotationSettingsBuilder.VerticalTextPosition |
verical text postion type
|
ImportEclassMappingMode |
enum for import eClass mapping mode.
|
ImportType |
Definition of the EClass mapping behaviour types
|
InstanceDataBlockBuilder.ActionType |
the idb scope
|
InstanceDataBlockBuilder.CreateMode |
the idb create mode
|
InstantiateTemplateBulkBuilder.PlacementType |
Choices for placement type, can be Place in Navigator or Place on Page
|
InterfaceAccessType |
The Plc Interface Access types
|
InterruptionPointBuilder.Variant |
Represents Interruption Point Variant type
|
LineDesignerMappingBuilder.FilterType |
enum for the filter
|
LoadLineDesignerBuilder.RevisionRuleType |
enum for the revision rule
|
Manage2dSymbolsBuilder.SymbolRepresentationTypes |
Representation type of symbol
|
MemorySectionType |
Definition of the memory section types
|
MountingInterfaceBuilder.FixingPolicy |
Represents component fixing type
|
MountingInterfaceBuilder.InterfaceType |
Represents mounting interface type
|
MountingInterfaceBuilder.ReceptaclePolicy |
Represents component receptacle type
|
MultiValueObjectsPort.JaAmeValueObjectUsageType |
type which usagetype has to be used
|
NamingRuleSettingsBuilder.Sources |
different types of Delimiter sources
|
OperandRuleBuilder.CreationType |
replace or insert rule Type
|
OperatorRuleBuilder.NegationValue |
Enum of negation value
|
OperatorRuleBuilder.ParameterType |
Enum of parameter type
|
OpticalAnnotationSettingsBuilder.AnnotationAttrType |
Represents the type of annotations
|
OrderAspectsBuilder.OrderType |
possible choices for order of navigator objects
|
OrderAspectsBuilder.SortType |
possible choices for sorting of navigator objects in a set
|
PageBuilder.Types |
Represents the type of page
|
ParameterRuleBuilder.Connection |
connection Type
|
PlcDataType |
Definition of the PLC data types
|
PlcDataTypeSource |
Definition of the data type sources
|
PlcRule.RefObjectType |
type which discribed the context object
|
PlcRule.ReplacementType |
type which defined wich object has to be replaced
|
PlcRule.Type |
replace or insert rule Type.
|
PlcSymbolsEvaluatorBuilder.FilterType |
choices for type filter, can either be tags, instance dbs, function blocks, functions, eplan macros, or all
|
PortBuilder.ConnectableAttrProxyObjectType |
Represents the type of connectable attribute proxy object for typed port
|
PortBuilder.CreationModeType |
Represents the type of creation mode
|
PortBuilder.Type |
the type of a port
|
ProductMatchingRulesBuilder.Condition |
Represents matching rule condition
|
ProductSelectionBuilder.Type |
the product type for product selection
|
ProgrammingLanguage |
The Plc Programming Languages
|
QueryBuilder.Types |
the creation type of query
|
ReferenceObjectBuilder.SourceSelectionType |
possible choices for source object selection
|
SelectAMEBaseNode.ValueData |
This class holds the data returned from
SelectAMEBaseNode.getValue() |
SelectAMEBaseNode.ValueWithCaeSetObjectInfoData |
This class holds the data returned from
SelectAMEBaseNode.getValue() |
SelectAMEBaseNode.ValueWithSnapData |
This class holds the data returned from
SelectAMEBaseNode.getValue() |
SelectAMEExtendedObject.ValueData |
This class holds the data returned from
SelectAMEExtendedObject.getValue() |
SelectAMEExtendedObject.ValueWithCaeSetObjectInfoData |
This class holds the data returned from
SelectAMEExtendedObject.getValue() |
SelectAMEExtendedObject.ValueWithSnapData |
This class holds the data returned from
SelectAMEExtendedObject.getValue() |
SelectAMEPort.ValueData |
This class holds the data returned from
SelectAMEPort.getValue() |
SelectAMEPort.ValueWithCaeSetObjectInfoData |
This class holds the data returned from
SelectAMEPort.getValue() |
SelectAMEPort.ValueWithSnapData |
This class holds the data returned from
SelectAMEPort.getValue() |
SelectAndHighlightBuilder.SelType |
possible choices for selecting of navigator objects in a set
|
SelectAspectNode.ValueData |
This class holds the data returned from
SelectAspectNode.getValue() |
SelectAspectNode.ValueWithCaeSetObjectInfoData |
This class holds the data returned from
SelectAspectNode.getValue() |
SelectAspectNode.ValueWithSnapData |
This class holds the data returned from
SelectAspectNode.getValue() |
SortingBlockBuilder.Order |
possible choices for order selection
|
SymbolAnnotationBuilder.Anchor |
Represents anchor of annotation
|
SymbolAnnotationBuilder.Orientation |
Represents orientation of annotation
|
SymbolAuthoringBuilder.Types |
Represents the type of symbol
|
TiaPortalProjectSettingsBuilder.TiaPortalVersionType |
represents TIA Portal Version type
|
TypeMappingBuilder.LoadData |
This class holds the data returned from
TypeMappingBuilder.load(java.lang.String) |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.