Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static SlugRetentionBuilder.Types |
SlugRetentionBuilder.Types.TYPE_FIRST |
static SlugRetentionBuilder.Types |
SlugRetentionBuilder.Types.TYPE_SECOND |
Modifier and Type | Method and Description |
---|---|
SlugRetentionBuilder.Types |
SlugRetentionBuilder.type()
Returns the type
License requirements: None. |
static SlugRetentionBuilder.Types |
SlugRetentionBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SlugRetentionBuilder.Types |
SlugRetentionBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SlugRetentionBuilder.Types[] |
SlugRetentionBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SlugRetentionBuilder.setType(SlugRetentionBuilder.Types type)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.