Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static MWMoldedPartValidationBuilder.AssignToRegion |
MWMoldedPartValidationBuilder.AssignToRegion.CAVITY_REGION
assign selected region faces to the Cavity region
|
static MWMoldedPartValidationBuilder.AssignToRegion |
MWMoldedPartValidationBuilder.AssignToRegion.CORE_REGION
assign selected region faces to the Core region
|
Modifier and Type | Method and Description |
---|---|
MWMoldedPartValidationBuilder.AssignToRegion |
MWMoldedPartValidationBuilder.regionAssignToRegionOption()
Returns the option for assigning the selected region faces to the cavity or core region on the Region Tab page.
|
static MWMoldedPartValidationBuilder.AssignToRegion |
MWMoldedPartValidationBuilder.AssignToRegion.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MWMoldedPartValidationBuilder.AssignToRegion |
MWMoldedPartValidationBuilder.AssignToRegion.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MWMoldedPartValidationBuilder.AssignToRegion[] |
MWMoldedPartValidationBuilder.AssignToRegion.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MWMoldedPartValidationBuilder.setRegionAssignToRegionOption(MWMoldedPartValidationBuilder.AssignToRegion regionAssignToRegionOption)
License requirements: ug_mold_design ("UG MOLD") OR ug_prod_des_advisor ("Product Design Advisor") OR prog_die_wizard ("UG/Progressive Die Wizard") OR die_engineering ("DIE ENGINEERING") OR ug_die_design ("Die Design") OR nx_electrode_wizard ("NX Electrode Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.