Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static TrimRegionBuilder.BoundaryOption |
TrimRegionBuilder.BoundaryOption.BODY_CURVE
select body/edge/curve as boundary object
|
static TrimRegionBuilder.BoundaryOption |
TrimRegionBuilder.BoundaryOption.TRAVERSE
use traverse loop to select boundary object
|
Modifier and Type | Method and Description |
---|---|
TrimRegionBuilder.BoundaryOption |
TrimRegionBuilder.boundaryType()
Returns the value of boundary type option, which specifies to use body or edge/curve as boundary object.
|
static TrimRegionBuilder.BoundaryOption |
TrimRegionBuilder.BoundaryOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimRegionBuilder.BoundaryOption |
TrimRegionBuilder.BoundaryOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimRegionBuilder.BoundaryOption[] |
TrimRegionBuilder.BoundaryOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimRegionBuilder.setBoundaryType(TrimRegionBuilder.BoundaryOption boundaryType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.