public static class TrimRegionBuilder.BoundaryOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BODY_CURVE
select body/edge/curve as boundary object
|
static int |
_TRAVERSE
use traverse loop to select boundary object
|
static TrimRegionBuilder.BoundaryOption |
BODY_CURVE
select body/edge/curve as boundary object
|
static TrimRegionBuilder.BoundaryOption |
TRAVERSE
use traverse loop to select boundary object
|
Modifier and Type | Method and Description |
---|---|
static TrimRegionBuilder.BoundaryOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimRegionBuilder.BoundaryOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimRegionBuilder.BoundaryOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final TrimRegionBuilder.BoundaryOption BODY_CURVE
public static final TrimRegionBuilder.BoundaryOption TRAVERSE
public static final int _BODY_CURVE
public static final int _TRAVERSE
public static TrimRegionBuilder.BoundaryOption valueOf(int value)
public static TrimRegionBuilder.BoundaryOption valueOf(String name)
public static TrimRegionBuilder.BoundaryOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.