Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static ElectrodeDeleteBuilder.Types |
ElectrodeDeleteBuilder.Types.COMPONENT
Delete electrode, holder and pallet.
|
static ElectrodeDeleteBuilder.Types |
ElectrodeDeleteBuilder.Types.SPARKING_BODY
Delete sparking body from electrode.
|
Modifier and Type | Method and Description |
---|---|
ElectrodeDeleteBuilder.Types |
ElectrodeDeleteBuilder.type()
Returns the object type to be deleted.
|
static ElectrodeDeleteBuilder.Types |
ElectrodeDeleteBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElectrodeDeleteBuilder.Types |
ElectrodeDeleteBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElectrodeDeleteBuilder.Types[] |
ElectrodeDeleteBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElectrodeDeleteBuilder.setType(ElectrodeDeleteBuilder.Types type)
License requirements: nx_electrode_wizard ("NX Electrode Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.