Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static ScrapDesignBuilder.AddonType |
ScrapDesignBuilder.AddonType.OVERCUT
Creates overcut
|
static ScrapDesignBuilder.AddonType |
ScrapDesignBuilder.AddonType.OVERLAP
Creates overlap
|
static ScrapDesignBuilder.AddonType |
ScrapDesignBuilder.AddonType.TRIMMING
Creates trimming
|
static ScrapDesignBuilder.AddonType |
ScrapDesignBuilder.AddonType.USER_DEFINED
Creates user defined add-on
|
Modifier and Type | Method and Description |
---|---|
ScrapDesignBuilder.AddonType |
ScrapDesignBuilder.addonOperation()
Returns the add-on operation, which includes overlap, overcut, trimming and user defined
License requirements: None. |
static ScrapDesignBuilder.AddonType |
ScrapDesignBuilder.AddonType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ScrapDesignBuilder.AddonType |
ScrapDesignBuilder.AddonType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ScrapDesignBuilder.AddonType[] |
ScrapDesignBuilder.AddonType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ScrapDesignBuilder.setAddonOperation(ScrapDesignBuilder.AddonType addonOperation)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.