Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static ElectrodeBlankBuilder.BlankMaterial |
ElectrodeBlankBuilder.BlankMaterial.COPPER
the material of the blank is copper
|
static ElectrodeBlankBuilder.BlankMaterial |
ElectrodeBlankBuilder.BlankMaterial.GRAPHITE
the material of the blank is graphite
|
Modifier and Type | Method and Description |
---|---|
ElectrodeBlankBuilder.BlankMaterial |
ElectrodeBlankBuilder.material()
Returns the material of the blank.
|
static ElectrodeBlankBuilder.BlankMaterial |
ElectrodeBlankBuilder.BlankMaterial.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElectrodeBlankBuilder.BlankMaterial |
ElectrodeBlankBuilder.BlankMaterial.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElectrodeBlankBuilder.BlankMaterial[] |
ElectrodeBlankBuilder.BlankMaterial.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElectrodeBlankBuilder.setMaterial(ElectrodeBlankBuilder.BlankMaterial material)
License requirements: nx_electrode_wizard ("NX Electrode Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.