Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static MWDefineSheetsBuilder.DefineStepType |
MWDefineSheetsBuilder.DefineStepType.CAVITYAND_CORE |
static MWDefineSheetsBuilder.DefineStepType |
MWDefineSheetsBuilder.DefineStepType.CUT_SOLIDS |
Modifier and Type | Method and Description |
---|---|
MWDefineSheetsBuilder.DefineStepType |
MWDefineSheetsBuilder.defineStep()
Returns the define step for defining Cavity and Core using the Split Body method
License requirements: None. |
static MWDefineSheetsBuilder.DefineStepType |
MWDefineSheetsBuilder.DefineStepType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MWDefineSheetsBuilder.DefineStepType |
MWDefineSheetsBuilder.DefineStepType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MWDefineSheetsBuilder.DefineStepType[] |
MWDefineSheetsBuilder.DefineStepType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MWDefineSheetsBuilder.setDefineStep(MWDefineSheetsBuilder.DefineStepType defineStep)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.