Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static InsertAuxiliaryBuilder.RampStepsType |
InsertAuxiliaryBuilder.RampStepsType.ADD_MATERIAL |
static InsertAuxiliaryBuilder.RampStepsType |
InsertAuxiliaryBuilder.RampStepsType.CREATE_CURVES_AND_DIVIDE_FACE |
static InsertAuxiliaryBuilder.RampStepsType |
InsertAuxiliaryBuilder.RampStepsType.CREATE_RAMP |
static InsertAuxiliaryBuilder.RampStepsType |
InsertAuxiliaryBuilder.RampStepsType.DELETE_RAMP |
Modifier and Type | Method and Description |
---|---|
InsertAuxiliaryBuilder.RampStepsType |
InsertAuxiliaryBuilder.rampSteps()
Returns the ramp steps
License requirements: None. |
static InsertAuxiliaryBuilder.RampStepsType |
InsertAuxiliaryBuilder.RampStepsType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InsertAuxiliaryBuilder.RampStepsType |
InsertAuxiliaryBuilder.RampStepsType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InsertAuxiliaryBuilder.RampStepsType[] |
InsertAuxiliaryBuilder.RampStepsType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InsertAuxiliaryBuilder.setRampSteps(InsertAuxiliaryBuilder.RampStepsType rampSteps)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.