Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static PunchInsertBuilder.PunchPocketTypeItemsBackingPlate |
PunchInsertBuilder.PunchPocketTypeItemsBackingPlate.CIRCLE
Punch pocket type in backing plate is circle
|
static PunchInsertBuilder.PunchPocketTypeItemsBackingPlate |
PunchInsertBuilder.PunchPocketTypeItemsBackingPlate.CLEARANCE
Punch pocket type in backing plate is clearance
|
static PunchInsertBuilder.PunchPocketTypeItemsBackingPlate |
PunchInsertBuilder.PunchPocketTypeItemsBackingPlate.FILLET
Punch pocket type in backing plate is fillet
|
static PunchInsertBuilder.PunchPocketTypeItemsBackingPlate |
PunchInsertBuilder.PunchPocketTypeItemsBackingPlate.SUPER_OFFSET
Punch pocket type in backing plate is super offset
|
Modifier and Type | Method and Description |
---|---|
PunchInsertBuilder.PunchPocketTypeItemsBackingPlate |
PunchInsertBuilder.punchPocketTypeInBackingPlate()
Returns the punch pocket type in backing plate.
|
static PunchInsertBuilder.PunchPocketTypeItemsBackingPlate |
PunchInsertBuilder.PunchPocketTypeItemsBackingPlate.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PunchInsertBuilder.PunchPocketTypeItemsBackingPlate |
PunchInsertBuilder.PunchPocketTypeItemsBackingPlate.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PunchInsertBuilder.PunchPocketTypeItemsBackingPlate[] |
PunchInsertBuilder.PunchPocketTypeItemsBackingPlate.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PunchInsertBuilder.setPunchPocketTypeInBackingPlate(PunchInsertBuilder.PunchPocketTypeItemsBackingPlate punchPocketTypeInBackingPlate)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.