Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Method and Description |
---|---|
ShimInnerProfileSetBuilder |
ShimBuilder.createInnerProfileSetBuilder()
Create a inner profile set builder object.
|
ShimInnerProfileSetBuilder |
ProgressiveDieManager.createShimInnerProfileSetBuilder()
Creates a
ShimInnerProfileSetBuilder
License requirements: None. |
ShimInnerProfileSetBuilder |
ShimInnerProfileSetBuilderList.findItem(int index)
Returns the object at the input index.
|
ShimInnerProfileSetBuilder[] |
ShimInnerProfileSetBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ShimInnerProfileSetBuilderList.append(ShimInnerProfileSetBuilder object)
Appends an object to the list
License requirements: None. |
void |
ShimInnerProfileSetBuilderList.append(ShimInnerProfileSetBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ShimInnerProfileSetBuilderList.erase(ShimInnerProfileSetBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
ShimInnerProfileSetBuilderList.erase(ShimInnerProfileSetBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ShimInnerProfileSetBuilderList.findIndex(ShimInnerProfileSetBuilder obj)
Finds the index where the input object appears.
|
void |
ShimInnerProfileSetBuilderList.insert(int location,
ShimInnerProfileSetBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
ShimInnerProfileSetBuilderList.setContents(ShimInnerProfileSetBuilder[] objects)
Sets the contents of the entire list.
|
void |
ShimInnerProfileSetBuilderList.swap(ShimInnerProfileSetBuilder object1,
ShimInnerProfileSetBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.