Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static FormingInsertBuilder.DesignOptions |
FormingInsertBuilder.DesignOptions.FORMING_DIE
design the forming die
|
static FormingInsertBuilder.DesignOptions |
FormingInsertBuilder.DesignOptions.FORMING_PUNCH
design the forming punch
|
Modifier and Type | Method and Description |
---|---|
FormingInsertBuilder.DesignOptions |
FormingInsertBuilder.designOption()
Returns the design option to design punch or die.
|
static FormingInsertBuilder.DesignOptions |
FormingInsertBuilder.DesignOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FormingInsertBuilder.DesignOptions |
FormingInsertBuilder.DesignOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FormingInsertBuilder.DesignOptions[] |
FormingInsertBuilder.DesignOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FormingInsertBuilder.setDesignOption(FormingInsertBuilder.DesignOptions designOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.