Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static StripLayoutBuilder.FromStationType |
StripLayoutBuilder.FromStationType.ONE
the beginning layout station is 1
|
static StripLayoutBuilder.FromStationType |
StripLayoutBuilder.FromStationType.THREE
the beginning layout station is 3
|
static StripLayoutBuilder.FromStationType |
StripLayoutBuilder.FromStationType.TWO
the beginning layout station is 2
|
Modifier and Type | Method and Description |
---|---|
StripLayoutBuilder.FromStationType |
StripLayoutBuilder.fromStation()
Returns the From Station type on the Layout group of Strip Layout Design dialog
License requirements: None. |
static StripLayoutBuilder.FromStationType |
StripLayoutBuilder.FromStationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StripLayoutBuilder.FromStationType |
StripLayoutBuilder.FromStationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StripLayoutBuilder.FromStationType[] |
StripLayoutBuilder.FromStationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StripLayoutBuilder.setFromStation(StripLayoutBuilder.FromStationType fromStation)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.