Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static MotionSimulationBuilder.EjectorMoveOptions |
MotionSimulationBuilder.EjectorMoveOptions.AFTER
Eject product after mold fully opened
|
static MotionSimulationBuilder.EjectorMoveOptions |
MotionSimulationBuilder.EjectorMoveOptions.WHILE
Eject product while mold opening
|
Modifier and Type | Method and Description |
---|---|
MotionSimulationBuilder.EjectorMoveOptions |
MotionSimulationBuilder.ejectorMoveOption()
Returns the ejector move option
License requirements: None. |
static MotionSimulationBuilder.EjectorMoveOptions |
MotionSimulationBuilder.EjectorMoveOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MotionSimulationBuilder.EjectorMoveOptions |
MotionSimulationBuilder.EjectorMoveOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MotionSimulationBuilder.EjectorMoveOptions[] |
MotionSimulationBuilder.EjectorMoveOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MotionSimulationBuilder.setEjectorMoveOption(MotionSimulationBuilder.EjectorMoveOptions ejectorMoveOption)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.