Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static StripLayoutStationInformationBuilder.StationItem |
StripLayoutStationInformationBuilder.StationItem.ONE
Define station number -- 01
|
static StripLayoutStationInformationBuilder.StationItem |
StripLayoutStationInformationBuilder.StationItem.THREE
Define station number -- 03
|
static StripLayoutStationInformationBuilder.StationItem |
StripLayoutStationInformationBuilder.StationItem.TWO
Define station number -- 02
|
Modifier and Type | Method and Description |
---|---|
StripLayoutStationInformationBuilder.StationItem |
StripLayoutStationInformationBuilder.stationNumber()
Returns the station number to define information
License requirements: None. |
static StripLayoutStationInformationBuilder.StationItem |
StripLayoutStationInformationBuilder.StationItem.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StripLayoutStationInformationBuilder.StationItem |
StripLayoutStationInformationBuilder.StationItem.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StripLayoutStationInformationBuilder.StationItem[] |
StripLayoutStationInformationBuilder.StationItem.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StripLayoutStationInformationBuilder.setStationNumber(StripLayoutStationInformationBuilder.StationItem stationNumber)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.