Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static PunchInsertBuilder.NormalClearanceOptionTypeItems |
PunchInsertBuilder.NormalClearanceOptionTypeItems.CONSTANT
The design option is normal
|
static PunchInsertBuilder.NormalClearanceOptionTypeItems |
PunchInsertBuilder.NormalClearanceOptionTypeItems.SUPER_OFFSET
The design option is fineblanking
|
static PunchInsertBuilder.NormalClearanceOptionTypeItems |
PunchInsertBuilder.NormalClearanceOptionTypeItems.VARIABLE
The design option is fineblanking
|
Modifier and Type | Method and Description |
---|---|
PunchInsertBuilder.NormalClearanceOptionTypeItems |
PunchInsertBuilder.normalClearanceOption()
Returns the clearance option for normal pierce design.
|
static PunchInsertBuilder.NormalClearanceOptionTypeItems |
PunchInsertBuilder.NormalClearanceOptionTypeItems.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PunchInsertBuilder.NormalClearanceOptionTypeItems |
PunchInsertBuilder.NormalClearanceOptionTypeItems.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PunchInsertBuilder.NormalClearanceOptionTypeItems[] |
PunchInsertBuilder.NormalClearanceOptionTypeItems.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PunchInsertBuilder.setNormalClearanceOption(PunchInsertBuilder.NormalClearanceOptionTypeItems normalClearanceOption)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.