Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static MotionSimulationBuilder.Types |
MotionSimulationBuilder.Types.ADD_KINEMATIC_MODEL
Adds kinematic model
|
static MotionSimulationBuilder.Types |
MotionSimulationBuilder.Types.MOUNT_COMPONENT
Mounts die components to kinematic components
|
Modifier and Type | Method and Description |
---|---|
MotionSimulationBuilder.Types |
MotionSimulationBuilder.type()
Returns the type to specify which operation of motion simulation takes effect.
|
static MotionSimulationBuilder.Types |
MotionSimulationBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MotionSimulationBuilder.Types |
MotionSimulationBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MotionSimulationBuilder.Types[] |
MotionSimulationBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MotionSimulationBuilder.setType(MotionSimulationBuilder.Types type)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.