Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DefineNeutralFactorBuilder.FormulaOptions |
DefineNeutralFactorBuilder.FormulaOptions.BEND_ALLOWANCE
Bend allowance formula use different formula according to inner bend radius and thickness
|
static DefineNeutralFactorBuilder.FormulaOptions |
DefineNeutralFactorBuilder.FormulaOptions.GENERAL
General formula use the ratio of inner bend radius and thickness
|
Modifier and Type | Method and Description |
---|---|
DefineNeutralFactorBuilder.FormulaOptions |
DefineNeutralFactorBuilder.neutralFactorFormula()
Returns the neutral factor formula option, decides which method used to calculate the neutral factor
License requirements: None. |
static DefineNeutralFactorBuilder.FormulaOptions |
DefineNeutralFactorBuilder.FormulaOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DefineNeutralFactorBuilder.FormulaOptions |
DefineNeutralFactorBuilder.FormulaOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DefineNeutralFactorBuilder.FormulaOptions[] |
DefineNeutralFactorBuilder.FormulaOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DefineNeutralFactorBuilder.setNeutralFactorFormula(DefineNeutralFactorBuilder.FormulaOptions neutralFactorFormula)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.